Questions & Answers
What is an air handler?
The air handler is an important part of your air conditioning equipment. Its job is to effectively circulate conditioned air throughout your home.
What It Is
Your central heating and cooling system consists of two main parts—an outdoor unit and an indoor unit, or air handler. When matched with a heat pump, it circulates both cool and hot air, depending on the season. With properly sized Trane air handlers, your family has the right amount of clean, comfortable air all year round. Plus, Trane air handlers make a significant contribution to the overall efficiency of your system. That’s because the more efficient your air handler is, the less work your outdoor unit has to do to make your home comfortable.
How It Works
The Hyperion™ air handler is built unlike anything the market has ever seen. It is constructed more like a refrigerator than a typical air handler, with insulation between the walls of the innovative cabinet. This insulation prevents condensation that may cause damage to the air handler itself or your home. In addition to eliminating “sweating,” the cabinet also eliminates the loose fibers from fiberglass insulation that may enter the airstream with other air handlers. The exclusive double-wall construction provides families with peace of mind and cleaner, safer indoor air.