Questions & Answers

Questions or Live Chat

What is Snowball II?

Snowball II is the nickname for the durable Climatuff® compressor at Trane’s SEET testing facility. It’s named for the block of ice it has encased itself in by running nonstop since 2000, and still is today.

What It Is
Snowball II lives at the Trane SEET lab in Tyler, Texas. SEET stands for Systems Extreme Environmental Test, where the durable Climatuff® compressor is constantly running, enduring extreme heat and cold, working tirelessly at high pressure levels and proving that it really is hard to stop a Trane.

What happened to Snowball I?
The original Snowball, also a Climatuff® compressor, began its life in late 1972, running nearly 28 years under the same SEET lab standards and encasing itself in a ball of ice. It ran at an estimated 3500 rpm, equaling an automobile running between 60 and 70 miles per hour, covering 14.8 million miles. Now, that’s a road trip.

The funny story behind Snowball is that it showed up at the lab “DOA” for some unexplained reason, but when it was started up it ran fine. Not just fine, it ran great. Well, what do you do with a compressor that’s running great? At the Trane SEET lab, you re-weld it and put it into continuous flood test mode. Five presidents later and after seeing the rise and fall of disco, glam rock and grunge music, Snowball finally ran out of steam, but left a legacy in the name of the patented Trane Climatuff® compressor found in every Trane heat pump and air conditioner today.

Related Questions

  1. 1 What is the history of Trane?
  1. 2 How many patents does Trane have?
  1. 3 What is Climatuff®?

Have more Questions? Talk to an Expert.

Trane - Comfort Specialist
Expanded links