ne

Questions & Answers

Questions or Live Chat

How clean is the air in my home?

In general, indoor air is four to five times more polluted than outdoor air. Approximately 87% of American homeowners are unaware of indoor air pollution.

Get to Know Particulates

There’s more in the air than you can easily see—particles, dust and smoke, all of them potential triggers for asthma and allergy attacks. Particles like dust, smoke and bacteria are often .3 microns or less. At that size, allergens can get deep into your lungs because they aren’t filtered well by your nose and throat.

Reduce Particulates with an Air Cleaning System

An effective whole-house air cleaner, such as Trane CleanEffects™, can reduce the presence of potential asthma and allergy attack triggers in your home. Get rid of the majority of particles like dust, pollen, pet hair and dander, dust mites, mildew, lint, fungus, most tobacco smoke, cooking grease, and even bacteria.

Did You Know?

  • According to a study by the Commonwealth of Massachusetts, indoor air contaminants are responsible for or aggravate half of all illnesses.
  • Poor indoor air quality negatively affects more than 15 million Americans who have asthma and the 28 million who suffer from hay fever and other allergies.
  • It is recommended we drink approximately two quarts of clean water each day. By comparison, we inhale approximately 15,000 quarts of air each day.
  • More than 15 million Americans are estimated to have asthma, including one in 13 school-age children.
  • Because they breathe faster than adults, children inhale 50% more air per pound
    of body weight than adults and are especially sensitive to air quality problems.

Related Questions

  1. 1 How can I make the air in my home cleaner?
  1. 2 What is Trane CleanEffects™?
  1. 3 What is a micron?

Have more Questions? Talk to an Expert.

Trane - Comfort Specialist
Expanded links