Trane
Find a dealer   Make a dealer appointment
 
Products Menu
arrowIntroduction
arrowAir Conditioners
arrowCompare Air Conditioners
arrowUltra Efficiency Units
arrowSuper Efficiency Units
arrowHigh Efficiency Units
arrowStandard Efficiency Units
arrowGuide to Cooling
arrowHeat Pumps
arrowAir Cleaners
arrowThermostats
arrowFurnaces & Coils
arrowAir Handlers
arrowHumidifiers
arrowCommunicating Systems
arrowPackaged Units
arrowBoilers
arrowFrequently Asked Questions
arrowGlossary
print this page
For Maximum Comfort, Replace Entire Central Air System, Not Just Half of It

If you're thinking about increasing the comfort level of your home by replacing your old central air conditioning or heat pump system with a new high efficiency one, be sure to replace the entire system, not just half of it. Otherwise, you may not get the performance you expect. So states the Trane Home Comfort Institute, a consumer information service on heating and cooling.

According to the Institute, most central air and heat pump systems are "split" systems, meaning they consist of two halves: an indoor unit or coil that pulls heat from inside air; and an outdoor unit or condenser that releases that heat to the outside air.

To obtain optimum energy saving and comfort levels, the indoor and outdoor units should be replaced at the same time. Far too often homeowners only replace the outdoor unit and neglect replacing the indoor unit. As a result, the new system doesn't always live up to their expectations.

They don't get the desired results because the indoor and outdoor units are designed to work as a team. They are matched in both capacity and efficiency when first installed and should be matched again when replaced.

Replacing an old outdoor unit with a new high efficiency model without replacing the indoor unit with an equally efficient model will simply not produce the desired performance.

Replacing both units will increase the initial cost of replacing the system. However, Trane Home Comfort Institute experts say the increase in energy savings, comfort level and overall reliability is well worth the investment.

Your feedback matters
Your comfort is our #1 priority. Tell us how we can serve you better.
Take our Web site survey
Find Your Ideal System
Use the Trane System Customizer to choose a system based on your unique comfort requirements
Learn more
An in-depth look at air conditioners
Get more information on choosing the right air conditioner for your home.
Guide to cooling
Purchasing and financing options
See how you can work with your dealer to make your next home comfort unit a Trane.
Purchasing and financing
Why choose Trane?
Learn how quality makes all the difference for your family's total home comfort.
Clean Air is Trane Air™
The True Trane
Difference
DID YOU KNOW?
Did You Know
dyk_take_the_quiz_button.gif
See how TRANE
CleanEffects™ works
Trane Residential is a leading global provider of indoor comfort systems. Trane’s offerings include energy-efficient cooling and heating solutions for homes, air conditioners, heat pumps, furnaces, air humidifiers, thermostats, parts and service.
© 2008 Trane Inc.  All rights reserved