How a Central Heating and
Cooling Air Conditioning System Works
Central cooling
What it is
The most common central cooling system is a split system, which includes an outdoor cabinet containing a condenser coil and compressor, and an indoor evaporator coil, usually installed in conjunction with your furnace or air handler. The compressor pumps a chemical called refrigerant through the system.
How it works
Once warm air inside your home blows across the indoor evaporator coil, its heat energy transfers to the refrigerant inside the coil. That transfer, in turn, “cools” the air. The refrigerant is pumped back to the compressor where the cycle begins again. The heat absorbed by the refrigerant is moved outside your home while cooled air is blown inside. Moisture that contributes to humidity is also condensed out of the air.
Your cooling system is usually combined with your central heating system because they share the same ductwork for distributing conditioned air throughout your home.
Central heating
What it is
Central heating systems have a primary heating appliance, such as a furnace, typically located in your basement or garage. All furnaces consist of four main components: 1) burners that deliver and burn fuel, 2) heat exchangers, 3) a blower and 4) a flue that acts as an exhaust for gaseous by-products. Depending on your situation, region and needs, you can choose from heating systems running on either gas or oil as fuel, or a hybrid packaged system that can use both fuel types.
How it works
Combustion gases are generated by the burners in your furnace and passed over a heat exchanger. Air from your home blows across the heat exchanger to be warmed. It is then blown through a system of ducts to distribute around your home.
During warm seasons your heating system works with your central air conditioning. Air is cooled as it’s blown over your air conditioning unit’s cooling coil, often attached to the exhaust of the furnace, and then sent over the same air ducts throughout your home.
An independent Trane dealer can help you decide which central cooling and heating system is right for you. Trane matched systems can be customized with cooling and heating units that match your situation and let you choose from a range of energy efficiency.
Trane DealerMatched Systems
Links



Our helpful guide shows you how to find the right matched system for your home.
Make sense of HVAC jargon and technical terms.