TRANE FOR:
ARCHITECTS
DATA CENTERS
ENGINEERS
HEALTHCARE
HIGHER EDUCATION
K12 EDUCATION
 

VariTrane™ Duct Designer

FAQ - Varitrane™ Duct Designer

Frequently asked questions...

FAQ  June 2000

Read about:

Can Duct Configurator model return or exhaust ductwork?
How can Duct Configurator model a plug fan in a plenum?
Can I get sound information?
Must I end with a VAV box or diffuser?
Why do some sections exceed my pre-set maximum velocity?
How do I transition from rectangular to oval ductwork?
Static regain is not downsizing my duct sections enough resulting in very low velocities. What is going on?
Why after changing the minimum velocity, are my velocities still too low?
Why is my airflow increasing as I move away from the fan?

Can Duct Configurator model return or exhaust ductwork?
No. To model return or exhaust ductwork, use both the Ductulator and the Fitting Loss Calculator. The resultant static pressure can be used on the fan tab as "SP through equipment and return."

Top

How can Duct Configurator model a plug fan in a plenum?
Refer to the help file on "plug fan."

Top

Can I get sound information?
No. The next release will include sound information.

Top

Must I end with a VAV box or diffuser?
Yes, Duct Configurator requires an end device at every outlet on the system.

Top

Why do some sections exceed my pre-set maximum velocity?
There are several possibilities. Most commonly, exceeding the maximum occurs in a section that leads to a VAV box or a diffuser. When creating a VAV box or diffuser using duct designer, enter the inlet diameter. The diameter specified becomes the immediate upstream section’s diameter as well. With the size of that section determined, the velocity is simply a result of the diameter and cfm. A similar situation exists at the fan. The next section is the same size as the fan.

Top

How do I transition from rectangular to oval ductwork?
This is a two step process. You must first transition to round and then transition to oval. There is no direct transition to change shape from rectangular to oval.

Top

Static regain is not downsizing my duct sections enough resulting in very low velocities. What is going on?
Static regain attempts to maintain the same static pressure throughout the duct system by recovering static pressure from velocity pressure. To do this, it slows the velocity down by keeping the duct sizes large. We defined a minimum velocity setting in the .ini file that allows you to set the minimum velocity Duct Designer will uses to determine when to downsize the section.

To change the 500 fpm default in the program you need to modify the duct_dsn.ini file. Click start menu and type "duct_dsn.ini" to view the ini file. Look for a section labeled "[velocity]"; if velocity is not there add it as shown.

e.g.
[velocity]
limit = 1500
This example sets the minimum velocity for static calculations to 1500 fpm. Change the "limit" in the ini to provide greater flexibility in attaining your needed velocity requirements. In version 3.0 or Duct32, there is an advanced features to set this number.

Top

Why after changing the minimum velocity, are my velocities still too low?
The reason is that when the program reaches the minimum setting, it has an associated actual (not nominal) ductsize at that moment. For example, the Duct Designer sees that the 500fpm minimum has been reached, and the duct size happens to be 5.2 inches in diameter. Since 5.2 inches is not a standard size of ductwork, Duct Designer chooses the next LARGER duct size, which is 6 inches. The velocity will then dip slightly below the 500fpm minimum.

Top

Why is my airflow increasing as I move away from the fan?
You have entered a diversity factor for a VAV system. At the fan, the airflow will be less than the sum of airflow at the boxes. Size the sections leading out the boxes for the maximum peak airflow. Size the trunk section only for the maximum block airflow. Size sections going to the VAV boxes for the peak airflow.

Top

 

OrderVariTrane Duct Designer
  Locate a Trane Sales Office
Software Updates

Software Updates

Download software updates for Trane Controls.

Order Software

Order Software

Order C.D.S. Software now.
View license agreement.
Online order form.
Online GSA order form.
Faxable order form.

Training

Training

Learn how to maximize the benefits from Trane’s C.D.S. Design & Analysis software.
More...

    High Performance Buildings

    High Performance Buildings

    See how Trane helps you create and sustain High Performance Buildings for Life™.
    More...

      C.D.S. Software Central

      C.D.S. Software Central

      Support references for our C.D.S. Software suite.
      More...