Bethel Middle School
Trane recommended Trane’s PACT™ to Bryant School District
• $11.3 Million in Projected Energy and Operating Savings Over Life of Building
• USGBC LEED Certified
• Improved Staff and Student Comfort
The Bryant School District had already obtained bond funds to construct a new, conventional middle school. However, after school
district leadership began studying sustainable building features, with help from the local chapter of the U.S. Green Building Council (USGBC), the school district decided to change from a
conventionally designed school to a high performance, LEED-certified green building.
Trane recommended that the Bryant School District take advantage of Trane’s PACT™ (Performance
Agreement for Comfort from Trane) performance contracting program that would allow the school district to add green, sustainable building features to the new Bethel Middle School project. The PACT
agreement supplemented the already tight conventional construction budget with an additional $987,000 to cover the cost of all HVAC equipment plus a Trane Tracer Summit™ building automation system, lighting controls, daylight harvesting control, energy modeling, green power credits and all fees associated with LEED certification.
Bethel Middle School was built using the latest in HVAC, building automation, window and lighting
systems technology. As a result, Bethel Middle School is projected to save the school district $11.3 million in energy and operating costs over the life of the building - savings that can be put to use in education. The high efficiency HVAC systems and use of adequate ventilation air, combined with the
Tracer Summit automation system provides better indoor air quality and more consistent, comfortable room temperatures for teachers and students - for a positive impact on student learning.
Dr. Richard Abernathy, Bryant School District Superintendent and a leading proponent of including green, high efficiency features at Bethel Middle School, said, "Trane was instrumental in moving us closer to our goal of achieving LEED certification through the most energy efficient equipment, an
integrated control system and a performance contract that helped finance the new construction in accordance with enabling state legislation."
Another recent construction project by the Bryant School District, Hurricane Elementary School, also uses Trane HVAC systems.
In addition to state-of-the-art systems from Trane, Bethel Middle School includes such green features as
north-south exposure, combination concrete and steel construction, insulation, large roof overhangs, high-performance window glazing, high efficiency lighting, daylight
harvesting and low-impact landscaping.
- Trane Tracer Summit™ building automation system for integrated climate, lighting, energy use, scheduling, and other control features.
- Nearly 100 VariTrane™ VAV terminals include the patented Trane Flow Ring and Trane DDC controller.
- Trane XL16i two-stage condensing units (16 SEER) and variable speed air handlers.
|
|