Case Study - Industrial

American Crystal Sugar Company

Trane HVAC Systems, Heating And Air Conditioning, American Crystal Sugar Company - Industrial | Trane Download PDF | Print

A Sweet Solution

American Crystal Sugar Company(ACSC) has improved profitability and prevented spoilage of thousands of tons of sugarbeets through the use of Trane chillers and Calmac ice mats.

Challenge

Each year ACSC refines millions of tons of sugar beets (10 million tons in 2007) into sugar. The sugar beets are harvested each fall and placed in huge outdoor piles 880-feet long by 225-feet wide and 32-feet high. Each pile is worth approximately $5 million. The sugarbeets stay frozen through out the sub-freezing North Dakota Winter and ACSC processes these piles from September through May to refine the sugarbeats into sugar until the piles are completed. A major factor in preserving the quality of each year sugar beet crop is cold winter weather. However faced with warm spring weather ACSC was concerned about a large crop and significant spoilage as sugarbeets thawed before they could be processed.

Solution

Borrowing from hockey and ice arena technology,the sugarbeets are covered with Calmac ice mats through which 10-degree glycol solution is pumped. The freezing solution is generated by ten 200- and 300-ton air-cooled chillers from Trane Rental Services. This keeps the sugarbeets frozen until ready for processing.

Results

Thanks to Trane rental chillers, ACSC eliminated significant spoilage and saved approximately $1 million worth of sugarbeets during the 2007 season. By working with Trane Rental Services, ACSC rents only the cooling capacity required and does not need to spend capital on permanent facilities and equipment. Dan Bernhardson, Director of Agriculture Operations for ACSC, said, “As a sugarbeet cooperative one of our biggest challenges is maintaining the sugarbeets that are in storage. The 2006 crop was the largest ever in terms of storage. Trane delivered the rental chillers on time in March, 2007, and set them up in less than optimal conditions temperatures in North Dakota were still below zero. We finished processing the 2006 crop by the beginning of June, 2007. The savings in reduced sugarbeet spoilage were significant.” Bernhardson added, “The biggest thing is to have a good chiller technician on hand. These chillers need to be running 24 hours a day, seven days a week. After we completed the sugarbeet processing we held a debriefing meeting and Trane was already considering ways to improve their performance with next season crop.”

About American Crystal Sugar Company

American Crystal Sugar Company is an agricultural cooperative involved in growing and processing of sugar beets and is owned by nearly 2,900 shareholder entities in the Red River Valley of Northwestern Minnesota and eastern North Dakota. ACSC employs about 1,700 full and part time employees and is the largest beet sugar producer in the United States. ACSC operates sugar factories at Crookston, East Grand Forks, and Moorhead, Minn., Drayton and Hillsboro, N.D.; and Sidney, Mont., under the name Sidney Sugars Incorporated. ACSC corporate headquarters and technical services facilities are located in Moorhead, Minnesota

THE SPECIFICS

Expand

Close

THE SPECIFICS

Building Specifications

Application

Food Processing

Project Team

American Crystal Sugar Company
Trane Fargo
Trane Rental Services

SYSTEMS INSTALLED:

Ten 200- and 300-ton air-cooled chillers from Trane Rental Services. All 10 chillers were provided with pumps, flex hose, and electrical cable.

Trane Rental Services provides temporary HVAC solutions for a variety of applications, including emergency and planned situations. As an HVAC industry leader, Trane is equipped to supply fast, reliable solutions for any occasion. Trane’s modern fleet of rental air- and water-cooled chillers, airconditioners, generators and accessories are prepped and ready to ship at a moment’s notice. Trane rental chillers with capacities of from a one-half ton portable cooler to thousands of tons of chilled water, are available from stocking locations in major cities across the UnitedStates, Canada, Mexico and PuertoRico. For more information on Trane Rental Services, please call 800-755-5115 or visit www.trane.com/rentalservices