Systems & services: Eleven Trane Precedent™ light commercial rooftop air conditioning units and Eleven Ice Energy Ice Bear thermal energy storage units
The new Park Marina building, housing the Social Security Administration, needed an efficient, sustainable HVAC system. The Imperial Group development company teamed with architect Nichols Melburg & Rossetto, Redding Electric Utility (REU), Trane, Ice Energy and Timberline Heating and Air to install eleven Ice Bear® energy storage units, each coupled with a Trane high-efficiency Precedent™ rooftop air conditioner.
The energy storage system helps to reduce ratepayer costs by shifting the air conditioning load to nighttime when energy costs less and the compressors run more efficiently.
Summers in Redding, about 225 miles north of San Francisco, are long, hot and dry. Developer Imperial Group and architect Nichols Melburg & Rossetto wanted to design the most comfortable and energy-efficient building
possible when they built the single-story, 21,000 square-foot Craftsman-style Park Marina Building.
Redding Electric Utility (REU), Trane, Ice Energy
and Timberline Heating and Air recommended
using highly-efficient HVAC units that,
combined with Ice Energy’s distributed energy
storage units, make possible load-shifting
strategies for even more energy savings. The air
conditioning system includes Trane
high-efficiency Precedent™ rooftop air
conditioners coupled with Ice Energy® Ice Bear™
energy storage units. What makes this a winning
solution is not only the inherent efficiency, but
with energy storage the air conditioning load
can be shifted to nighttime hours when
electricity is not only less expensive, but cleaner
to generate. The Ice Bear units generate ice in
their integral tanks during nighttime hours when
the cost to produce electricity in Redding is less
than during daytime hours. Also, the
compressors operate more efficiently during
cooler nighttime hours.
The Ice Bear energy storage units operate in two
modes: Ice Cooling and Ice Charging. During ice
charging, the Ice Bear units each freeze about
450 gallons of water. When fully frozen, the Ice
Bear condensing units shut off and the ice is
stored until its cooling energy is needed. As
daytime temperatures rise, the power
consumption of air conditioning rises along with
it, increasing peak demand. During this peak
window, typically from noon to 6:00 p.m., the
Ice Bear unit switches to Ice Cooling mode,
replacing the energy intensive compressors in
the air conditioning units. The Ice Bear units
slowly melt the ice to provide building air
conditioning. A small, high-efficiency pump
pushes ice-cold R-410a refrigerant through an
Ice-Coil™ installed in each Trane unit. The
stored ice lasts for at least six hours. When fully
melted, building air conditioning is again
provided by the Trane air conditioning units.
During cool nighttime hours, the Ice Charge
mode is activated and the cycle begins again.
Greg Tropsa, co-founder and Executive Vice
President of Ice Energy, said, "The Ice Bear
program with REU is a win for everyone--
consumers enjoy air conditioned comfort, REU
meets its state-mandated goals to reduce peak
demand, the utility’s overall cost of service is
reduced, and the energy storage devices play an
important role in reducing California’s
greenhouse gas emissions. It’s a great example
of how to stimulate the local economy, create
jobs, and reduce environmental impact.”
Ice-Ready, Ice-Coil and Ice Bear are trademarks
of Ice Energy Corporation.
The single-story Park Marina Building, at 2660 Park Marina Drive
along the Sacramento River, comprises 21,000 square feet. In addition
to the energy storage system, the building features a white,
heat-reflecting roof and foot-thick, insulated concrete walls for
maximum energy efficiency. Paul Hauser, Director for REU (on left in
photo), stands near the Trane rooftop air conditioning units and the
Ice Bear energy storage units installed on the roof of the Park Marina
building. Projects like this serve the community’s electric needs safely
and reliably at very competitive energy rates.